some errors are reported when the official example is compiled

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

some errors are reported when the official example is compiled

ソリューションへジャンプ
1,959件の閲覧回数
johnsen_zhou
Contributor I

Hello:
   some errors are reported when the official example is compiled
   my computer has been rebooted.
   the c/c++ index has been rebuilt.
   thanks!

{19AFE6E2-B247-40E3-A7B9-DB9F56ECE78A}.png.jpg

タグ(3)
0 件の賞賛
返信
1 解決策
1,858件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

what about your .elf file, is built properly - can you see it in Binaries folder in your project?

If yes - you can try to refresh your project (right click on project name -> refresh (or F5 key)) and rebuild index: 

pastedImage_1.png

Then clean project and re-build it again. The error message should disappear. 

Jiri 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,859件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

what about your .elf file, is built properly - can you see it in Binaries folder in your project?

If yes - you can try to refresh your project (right click on project name -> refresh (or F5 key)) and rebuild index: 

pastedImage_1.png

Then clean project and re-build it again. The error message should disappear. 

Jiri 

0 件の賞賛
返信