some errors are reported when the official example is compiled

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

some errors are reported when the official example is compiled

跳至解决方案
1,358 次查看
johnsen_zhou
Contributor I

Hello:
   some errors are reported when the official example is compiled
   my computer has been rebooted.
   the c/c++ index has been rebuilt.
   thanks!

{19AFE6E2-B247-40E3-A7B9-DB9F56ECE78A}.png.jpg

标记 (3)
0 项奖励
回复
1 解答
1,257 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

what about your .elf file, is built properly - can you see it in Binaries folder in your project?

If yes - you can try to refresh your project (right click on project name -> refresh (or F5 key)) and rebuild index: 

pastedImage_1.png

Then clean project and re-build it again. The error message should disappear. 

Jiri 

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,258 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

what about your .elf file, is built properly - can you see it in Binaries folder in your project?

If yes - you can try to refresh your project (right click on project name -> refresh (or F5 key)) and rebuild index: 

pastedImage_1.png

Then clean project and re-build it again. The error message should disappear. 

Jiri 

0 项奖励
回复