s32k314 qspi sample code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

s32k314 qspi sample code

4,489件の閲覧回数
vasanth-sr
Contributor II

Hi 

how can i get the sample code of Qspi for s32k3xx.

i imported the s32k344 sample code from the RTD 2.0.1,But i am not able to add the peripheral's

 

Regards,

vasanth.

2 返答(返信)

4,472件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello Vasanth,

The peripherals are added using the Peripherals Tool. The QSPI Tool that you show in the images is an advanced tool which can be used to create customized parameters for the QuadSPI to be used by the BootROM. This is not supported for S32K3xx family of devices.

The available example applications are provided in the New Project from Example wizard:

mikedoidge_0-1671053176793.png

For specific details on the availability of QSPI example, I refer you to @namnguyenviet for further details.

Best Regards,

Mike

0 件の賞賛
返信

4,474件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @vasanth-sr 

At this point in time, S32DS 3.5 is not broadly supported on the S32K3 family. We do recommend to stay at version 3.4 until further notice.

 

B.R

VaneB

0 件の賞賛
返信