s32k3 sdk

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

s32k3 sdk

2,684件の閲覧回数
Anjalipurushothaman
Contributor III

I have installed s32ds.3.5 design studio IDE, the development kit I have received is s32k3X8EVB-Q289. In order to start with this I have looked into to install the s32k3 sdk from the extensions and updates but it's not available. please let me know from where I can install s32k3 sdk ?

 

 

0 件の賞賛
返信
2 返答(返信)

2,646件の閲覧回数
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @Anjalipurushothaman , 
I see that S32K3 SDK is unavailable in from the Add update side. We will fix this shortly. 

Till it is available, you can get the S32K3 SDK by following these steps: 

1. Select "Help", then "Install New Software "
Mehul_Patel_NXP_0-1684439929498.png

2. Then from the opened window, for "Work with" option - select the RTD from the drop down menu, 

Mehul_Patel_NXP_1-1684442833026.png

3. Then select the S32 Design Studio S32K3 SDK 

Mehul_Patel_NXP_2-1684442939514.png
Then you can install the S32K3 SDK. 

We will also work to fix the issue and make it available on S32DS Extension and Updates

Thank you. Best regards. 

- Mehul Patel

 

 

 

 

0 件の賞賛
返信

2,652件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @Anjalipurushothaman 

Correct me if I'm wrong, but what I understood was delivered a .zip file which is an update site for S32DS.

These files are installed as follows:

VaneB_0-1684437808361.png

Selects the DS_updatesite.zip you want to install.

Then in the same S32DS Extension and Updates tab you have to look for the update site you add previously select it and Install/Update.

With this, you should be able to use the software.

 

B.R.

VaneB

0 件の賞賛
返信