s32ds runtime error 216

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

s32ds runtime error 216

2,249 Views
esfrss
Contributor I

i tried change the setting of debugger

esfrss_0-1719556347155.png

but nothing change and A runtime error occurs "216"

is there any solution of this runtime error?

 

Labels (1)
0 Kudos
Reply
1 Reply

2,226 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @esfrss,

Is there a part of your application which needs this delay?

This configuration specifies a delay after the programmer resets the target that we check to see if the part has properly gone into background debug mode. This is normally useful if the target has a reset driver which hold the MCU in reset after the programmer releases the reset line.

Is there no communication when the value is set to default (0ms)?

Best regards,
Julián

0 Kudos
Reply