s32ds runtime error 216

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

s32ds runtime error 216

2,260件の閲覧回数
esfrss
Contributor I

i tried change the setting of debugger

esfrss_0-1719556347155.png

but nothing change and A runtime error occurs "216"

is there any solution of this runtime error?

 

ラベル(1)
0 件の賞賛
返信
1 返信

2,237件の閲覧回数
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @esfrss,

Is there a part of your application which needs this delay?

This configuration specifies a delay after the programmer resets the target that we check to see if the part has properly gone into background debug mode. This is normally useful if the target has a reset driver which hold the MCU in reset after the programmer releases the reset line.

Is there no communication when the value is set to default (0ms)?

Best regards,
Julián

0 件の賞賛
返信