s32 dessign studio SDK multicore project

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

s32 dessign studio SDK multicore project

1,340件の閲覧回数
kpdeshpande08
Contributor I

hi,
I am creating a project to run on multiple cores. Just for testing whether all the cores run in parallel I configured 3 user LEDs(one for each core) to blink continuously. First when i run program for coreZ4_0 and then when I run program for coreZ4_1, the LED configured for coreZ4_0 stops blinking. The same happens for CoreZ2. But only that after I run program for coreZ2, LED configured for CoreZ4_1 does not stop blinking. i.e. CoreZ4_1 and CoreZ2 can run parallel.
What might be the reason for the core getting blocked? Are there any additional settings that should be done?

タグ(3)
0 件の賞賛
返信
1 返信

1,214件の閲覧回数
raresvasile
NXP Employee
NXP Employee

Hi,

I have tried the scenario but I was not able to reproduce it.

Can you provide more details regarding SDK version, board and CPU used?

Can you share a small application which I can use to reproduce your actual code sequence?

Thank you,

Rares

0 件の賞賛
返信