s32 _3.4 demo compile error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

s32 _3.4 demo compile error

Jump to solution
2,606 Views
Lv_Jm
Contributor II
    • When I compile the demo project, the following error occurs.

      • How can I fix this error

    • QQ截图20230427105701.png

0 Kudos
Reply
1 Solution
2,540 Views
Lv_Jm
Contributor II

thanks,A few days ago, I formatted my laptop and reinstalled S32. The problem has been resolved, but thank you all the same.

View solution in original post

4 Replies
2,585 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @Lv_Jm 

did you click on Update Code icon in the configuration tool?

This is copied from the example description from user manual:

lukaszadrapa_0-1682573773593.png

 

The button can be found here:

lukaszadrapa_1-1682573858158.png

 

Regards

Lukas

0 Kudos
Reply
2,579 Views
Lv_Jm
Contributor II

I HAVE done that but it still have errors when compiling

0 Kudos
Reply
2,543 Views
mikedoidge
NXP Employee
NXP Employee

Hello,

This error doesn't appear to be the true source of the issue. The incremental build is complaining the object files are not found. Try performing a 'Clean Project' first, then a full build and share the errors that result.

mikedoidge_0-1682951355623.png

Best Regards,

Mike

0 Kudos
Reply
2,541 Views
Lv_Jm
Contributor II

thanks,A few days ago, I formatted my laptop and reinstalled S32. The problem has been resolved, but thank you all the same.