"An Internal error has occurred" when update example project on .mex file

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

"An Internal error has occurred" when update example project on .mex file

ソリューションへジャンプ
1,547件の閲覧回数
MVR
Contributor V

Hello everyone,

I'm trying to update an example about SPI, using S32K344 and S32DS 3.4. The SDK version is 2.0.1.

This is the error that I'm facing:

MVR_0-1730211965441.png

In the past I was not facing this error, but it started suddenly... What should I do?

Thank you,

MVR

0 件の賞賛
返信
1 解決策
1,520件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @MVR 

This error does not occur if you first removee SpiExternalDevice (SpiDriver tab) associated with SpiPhyUnit (SpiGeneral tab). 

Additionally, we recommend using the latest versions of RTD drivers in addition to the latest versions of the tools.

 

BR, VaneB

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,521件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @MVR 

This error does not occur if you first removee SpiExternalDevice (SpiDriver tab) associated with SpiPhyUnit (SpiGeneral tab). 

Additionally, we recommend using the latest versions of RTD drivers in addition to the latest versions of the tools.

 

BR, VaneB

0 件の賞賛
返信
1,537件の閲覧回数
MVR
Contributor V

I tried to reinstall the S32DS 3.4 and also the RTD S32K3XX 2.0.1 and still I'm facing the issue:

MVR_1-1730227660199.png

 

Basically I'm trying to remove the SpiPhyUnit_0 from the "Lpspi_Ip_HalfDuplexTransfer_S32K344" example...

0 件の賞賛
返信