processor expert

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

processor expert

Jump to solution
2,859 Views
indusivaraman
Contributor I

I read that processor expert is not supported on Linux or at least it may not work. can someone please tell me is there a workaround other than build the SW in Windows environment. what does the processor expert exactly do?

Labels (1)
0 Kudos
Reply
1 Solution
2,641 Views
raresvasile
NXP Employee
NXP Employee

Hi,

Indeed, ProcessorExpert is not supported under Linux environment. For S32 SDK, ProcessorExpert is used to generate the configuration structures that will help you configure the Peripheral Drivers much faster.

The workaround would be to use a Windows environment to generate the configuration structures and then to copy the into your project on the Linux machine.

Best regards,

Rares

View solution in original post

0 Kudos
Reply
1 Reply
2,642 Views
raresvasile
NXP Employee
NXP Employee

Hi,

Indeed, ProcessorExpert is not supported under Linux environment. For S32 SDK, ProcessorExpert is used to generate the configuration structures that will help you configure the Peripheral Drivers much faster.

The workaround would be to use a Windows environment to generate the configuration structures and then to copy the into your project on the Linux machine.

Best regards,

Rares

0 Kudos
Reply