processor expert

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,003件の閲覧回数
indusivaraman
Contributor I

I read that processor expert is not supported on Linux or at least it may not work. can someone please tell me is there a workaround other than build the SW in Windows environment. what does the processor expert exactly do?

ラベル(1)
0 件の賞賛
返信
1 解決策
2,785件の閲覧回数
raresvasile
NXP Employee
NXP Employee

Hi,

Indeed, ProcessorExpert is not supported under Linux environment. For S32 SDK, ProcessorExpert is used to generate the configuration structures that will help you configure the Peripheral Drivers much faster.

The workaround would be to use a Windows environment to generate the configuration structures and then to copy the into your project on the Linux machine.

Best regards,

Rares

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,785件の閲覧回数
raresvasile
NXP Employee
NXP Employee

Hi,

Indeed, ProcessorExpert is not supported under Linux environment. For S32 SDK, ProcessorExpert is used to generate the configuration structures that will help you configure the Peripheral Drivers much faster.

The workaround would be to use a Windows environment to generate the configuration structures and then to copy the into your project on the Linux machine.

Best regards,

Rares

0 件の賞賛
返信