printf function example for MPC5777C using s32 design studio

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

printf function example for MPC5777C using s32 design studio

3,975件の閲覧回数
vrushalitaklika
Contributor III

Hi,

Can someone help with example function for MPC5777C controller using s32 design studio?

Thanks

vrushali

3 返答(返信)

3,538件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

if you need printf for debug purposes - you can use for example ewl_c library with Debugger console: 

pastedImage_1.png

In debug settings enable semihosting:

pastedImage_2.png

You can see the print output in debug session console. 

Jiri

3,538件の閲覧回数
harsha_jakkamkr
Contributor II

Hi Jiri,

Is it possible to print with different colors on the console?

Regards,

Harsha

タグ(1)

3,538件の閲覧回数
harsha_jakkamkr
Contributor II

Works like a charm.

Thanks!

0 件の賞賛
返信