powerpc-eabivle.gdb.exe crashes during debug

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

powerpc-eabivle.gdb.exe crashes during debug

3,770 次查看
ronlewis
Contributor III

I am having issue debugging an application.  powerpc-eabivle.gdb.exe crashes while connecting to the MPC5644a.  Its only an issue on the one project, and will occasionally work.

IE: I can debug other projects without issue, but for one project it mostly fails and I can get it to connect occasionally.  I have compared the debugger settings and I don't see any differences.  

Has anyone seen this issue?  Any guidance?

标签 (1)
0 项奖励
回复
2 回复数

3,280 次查看
stanish
NXP Employee
NXP Employee

Hello Ron,

Could you possibly try to update Pemicro e200 debugging support plugin?

It includes some new features + some bug fixes.

See the instructions here: https://community.nxp.com/message/890477?commentID=890477#comment-890477 

Just select "GNU E200 PEMicro Interface Debugging Support" instead of ARM one

Please let us know it it helps.

Thanks!

Stan

0 项奖励
回复

3,280 次查看
ronlewis
Contributor III

The support plugins where already up to date.  I ended up creating a new project and coping the source files over to the new project and that fixed the issue.

0 项奖励
回复