powerpc-eabivle.gdb.exe crashes during debug

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

powerpc-eabivle.gdb.exe crashes during debug

4,965 Views
ronlewis
Contributor III

I am having issue debugging an application.  powerpc-eabivle.gdb.exe crashes while connecting to the MPC5644a.  Its only an issue on the one project, and will occasionally work.

IE: I can debug other projects without issue, but for one project it mostly fails and I can get it to connect occasionally.  I have compared the debugger settings and I don't see any differences.  

Has anyone seen this issue?  Any guidance?

Labels (1)
0 Kudos
Reply
2 Replies

4,475 Views
stanish
NXP Employee
NXP Employee

Hello Ron,

Could you possibly try to update Pemicro e200 debugging support plugin?

It includes some new features + some bug fixes.

See the instructions here: https://community.nxp.com/message/890477?commentID=890477#comment-890477 

Just select "GNU E200 PEMicro Interface Debugging Support" instead of ARM one

Please let us know it it helps.

Thanks!

Stan

0 Kudos
Reply

4,475 Views
ronlewis
Contributor III

The support plugins where already up to date.  I ended up creating a new project and coping the source files over to the new project and that fixed the issue.

0 Kudos
Reply