mpc5777c

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mpc5777c

3,605 Views
saichinnala
Contributor II

Hai,needed a example code for Esci module on mpc5777c with dual wire

 

0 Kudos
Reply
3 Replies

3,579 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Pay attention to MPC5 cookbook, example 15/16:
https://www.nxp.com/docs/en/application-note/AN2865.pdf

It is applicable also to MPC5777C as it used the same eSCI module.

I am using eSCI also for printf funtionity in the base project below:
https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/Example-MPC5777C-PinToggleStationery-GHS714/ta-p...

0 Kudos
Reply

3,571 Views
saichinnala
Contributor II

by adding your code am unable to build

@davidtosenovjan 

0 Kudos
Reply

3,443 Views
stanish
NXP Employee
NXP Employee

Hi,

I'm afraid the example was created for GreenHills development environment - Multi.

I'd suggest you to create a new S32DS multicore project (GCC compiler) and fit the relevant code to the pre-generated multicore project structure.

Hope it helps.

Stan 

0 Kudos
Reply