install S32 Design Studio IDE for ARM issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

install S32 Design Studio IDE for ARM issue

3,220件の閲覧回数
PhilChen007
Contributor I

when I install S32 Design Studio IDE for Arm, I meet the following problem. 

installation file is S32DS_ARM_Win32_v2.0_b170810.exe

my laptop OS is window7, 64-bit.  

please help to check what happened and how to solve it. Thank you. 2017-11-01_092744.pngs!

0 件の賞賛
返信
6 返答(返信)

2,861件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hello, 

did the Install shield started extracting files or error message pop up right after execution? Are you able get lnstallation log file -> located in [YOUR_INSTALL_PATH]\S32DS_ARM_v2.0\_S32 Design Studio for ARM v2.0_installation\Logs\ ?

Jiri

0 件の賞賛
返信

2,861件の閲覧回数
PhilChen007
Contributor I

Hi Jiri,

I check the Install shield can't started extracting files yet, when click the installation file, it enter into this below interface. 

2017-11-02_084444.png

after a while, the installation is stopped at the following picture. 2017-11-01_092744.png

I also don't find the installation directory which is [YOUR_INSTALL_PATH]\S32DS_ARM_v2.0\  at my laptop.  so can't got the lnstallation log file.   

Thanks. 

0 件の賞賛
返信

2,861件の閲覧回数
stanish
NXP Employee
NXP Employee

Phil,

1) Please make sure you have enough disk space on all the disc drives and enough of available RAM.

2) make sure that your TMP and TEMP folders are pointing to the same location:  

pastedImage_1.png

3) This error could also be due to a corrupt file associated with InstallAnywhere located in a Temp folder on the local machine. To correct the error, clear all files in the local Temp folders:

 C:\Temp

 C:\Windows\Temp

 C:\WINNT\Temp

 C:\Documents and Settings\\Local Settings\Temp

 C:\Users\\AppData\Local\Temp

Hope it helps.

Stan

0 件の賞賛
返信

2,861件の閲覧回数
PhilChen007
Contributor I

Hi Stan.

1, Disk space info as following, and my installed memory(RAM) is 8GB,   is it enough?  

pastedImage_7.png

2, TMP and TEMP folders are pointing to the location as below: 

pastedImage_2.png

3, clear all files in the local Temp folders.  

You mean is to delete all files in this folders?  if this will affect my operation system? 

Thanks for your help. 

Phil

0 件の賞賛
返信

2,861件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi Phil,

yes - you can delete all files from temp folders without affecting installed OS. Did you try download again the S32DS installer? The file itself may be corrupted. 

 

Jiri 

0 件の賞賛
返信

2,861件の閲覧回数
PhilChen007
Contributor I

Hi Jiri,

ok, I will try it according to your suggest.  Thank you.  

Phil 

0 件の賞賛
返信