i can not see example poject pin map

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i can not see example poject pin map

815 次查看
rlaxortn
Contributor IV

i am using s32ds 3.6.1version. rtd 4.0.0 , s32k344.

after i download rtd 4.0.0 and i open the porject. 

but i can not see example project pinmap. 

i got a message that project is old version., 

so i installed s32ds 3.5 version. but i get same issue. 

and i failed install s32ds 3.4 version. 

 

1. how i can see that project well? pin, driver, clock and so on. 

화면 캡처 2025-04-15 105527.png

 

2. i got a activation code for 3.4 version. but it is not work. 

how i can install s32ds 3.4 version ?

i already have install file s32ds 3.4version. i download in nxp.

 

thanks for regards. 

标记 (4)
0 项奖励
回复
1 回复

804 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

If it is a new project, it is recommended to use the latest S32K3 RTD 5.0.0 + S32DS v3.6.

Or refer to HOWTO: offline install S32K3 RTD 4.0.0 in S32DS v3.5

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复