how to program the S32K344 EVK in S32 design studio

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to program the S32K344 EVK in S32 design studio

9,662件の閲覧回数
Hareesh
Contributor II

Hello, NXP team

Our S32 design studio version is S32DS 3.5, and we are using the S32K344 EVK board.

The code is debugging correctly, however we are running into issues when we try to program the EVK board.

Kindly refer to the attached document.

Please assist me in fixing the problem.

 

Regards,

Hareesh

0 件の賞賛
返信
7 返答(返信)

9,559件の閲覧回数
Hareesh
Contributor II

Hi @VaneB ,

Please try just the ones created with the project, for example, Siul2_Port_Ip_Example_S32K344_Debug_FLASH_PNE.

Please find the attachments for your reference.

 

Best regards,

Hareesh

0 件の賞賛
返信

9,547件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @Hareesh 

The debug configurations are correct, but I saw that you have selected as the target device the S32K344 SECUREDEBUG. This configuration is only used when a JTAG key access is set. If you do not have secured JTAG access, use as the target device the S32K344. 

VaneB_1-1708938457081.png

VaneB_0-1708938430565.png

 

0 件の賞賛
返信

9,492件の閲覧回数
Hareesh
Contributor II

Hi @VaneB ,

 

For us debugging is working properly. But we are unable to program(run mode - see in attached screenshot) the micro controller.

 

Regards,

Hareesh

0 件の賞賛
返信

9,472件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @Hareesh 

Check the following community post. This topic was discussed there.

FLASH iSSUE ON S32K312_ MaxQFP172 

 

0 件の賞賛
返信

9,641件の閲覧回数
Hareesh
Contributor II

Hi @VaneB ,

Does this happen with the example codes or just with your code?

Yes, that is also the case with the example code and my code. For your reference, I've included a screenshot.

I've attached the screenshots for the debug settings as well. Kindly make use of it.

 

Best regards,

Hareesh

 

0 件の賞賛
返信

9,621件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @Hareesh 

According to the images shared, I saw that you have a bunch of debug configurations for the same project. Please try just the ones created with the project, for example, Siul2_Port_Ip_Example_S32K344_Debug_FLASH_PNE.

0 件の賞賛
返信

9,646件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @Hareesh 

Can you please share your debug session settings screen? Does this happen with the example codes or just with your code?

 

B.R.

VaneB

0 件の賞賛
返信