freemaster

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

freemaster

Jump to solution
5,407 Views
dongfang
Contributor II

Hello Sir:

                I  use the MPC5744P chip,and install the freemaster sofware. Now,it can already communicate normally.But, i  want to go further and use its active-X function. I use the example of user Manual about html.When I press the button, the interface will display an error message.Please help me to analyse . It would be better if you could provide a usable html routine.freemaster.png

0 Kudos
Reply
1 Solution
5,215 Views
petrfajmon-b173
NXP Employee
NXP Employee

Hello dongfang‌,

  please, can you share with me your FreeMASTER embedded and FreeMASTER PC projects for MPC5744P. It is difficult see the error reason.

Thank you,

Petr

View solution in original post

0 Kudos
Reply
4 Replies
5,215 Views
petrfajmon-b173
NXP Employee
NXP Employee

Hello dongfang

  look into the installed FreeMASTER  Communication Driver (FreeMASTER Communication Driver) example for ActiveX access from Excel. The default path to the example is: c:\NXP\FreeMASTER_Serial_Communication_Driver_V2.0\examples\ActiveX_examples\Excel\freemaster_excel.xlsm 

Best Regards,

Petr

0 Kudos
Reply
5,216 Views
petrfajmon-b173
NXP Employee
NXP Employee

Hello dongfang‌,

  please, can you share with me your FreeMASTER embedded and FreeMASTER PC projects for MPC5744P. It is difficult see the error reason.

Thank you,

Petr

0 Kudos
Reply
5,215 Views
dongfang
Contributor II

 Hello Sir,

              I want to use html to import the data from freemaster into the excel form. What should I do? Is there an example for easy access?

0 Kudos
Reply
5,215 Views
dongfang
Contributor II

.

Hello Petr,

Thank you very much for your reply.Attachment is my project file.Please help analyze the cause of the error.

I want to change the value of the variable when I press the button.But I have tried it failed a few times.I hope you can provide the routine.Looking forward to your reply.

Thank you,

dong fang

0 Kudos
Reply