error within code or some kind of incompatibility?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

error within code or some kind of incompatibility?

Jump to solution
1,578 Views
man_who_modifies_BMWs
Contributor I

I received an error when opening the HvBms400_775_722_TPL_Bring_Up example. 

Automotive package manager version 2024.01 was downloaded, the development package was downloaded, everything that should have been there was there. 

0 Kudos
Reply
1 Solution
1,557 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Please install SW32K3_RTD_4.4_R21-11_3.0.0_D2303 by refer to HOWTO: offline install S32K3 RTD 3.0.0 in S32DS v3.5


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,558 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Please install SW32K3_RTD_4.4_R21-11_3.0.0_D2303 by refer to HOWTO: offline install S32K3 RTD 3.0.0 in S32DS v3.5


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply