error sending an activation request to a remote activation server and processing the resulting

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

error sending an activation request to a remote activation server and processing the resulting

4,392件の閲覧回数
chai4896
Contributor I

error sending an activation request to a remote activation server and processing the resulting response.com. acresso. activation. handler. ServeException (FNP error 0)

0 件の賞賛
返信
1 返信

4,379件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello Chai,

Have you tried to activate with Offline method?

https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Activate-S32-Design-Studio/ta-p/...

It is possible that a firewall setting is blocking your PC from accessing the activation server. Sometimes this blocks the offline activation method, when performed from the same PC. You may need to use another PC, smartphone, tablet, or other device equipped with a web browser to perform the activation on the server, then transfer the resulting file to your PC for completion of the activation of S32 Design Studio.

Best Regards,

Mike