error sending an activation request to a remote activation server and processing the resulting

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

error sending an activation request to a remote activation server and processing the resulting

4,286 次查看
chai4896
Contributor I

error sending an activation request to a remote activation server and processing the resulting response.com. acresso. activation. handler. ServeException (FNP error 0)

0 项奖励
回复
1 回复

4,273 次查看
mikedoidge
NXP Employee
NXP Employee

Hello Chai,

Have you tried to activate with Offline method?

https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Activate-S32-Design-Studio/ta-p/...

It is possible that a firewall setting is blocking your PC from accessing the activation server. Sometimes this blocks the offline activation method, when performed from the same PC. You may need to use another PC, smartphone, tablet, or other device equipped with a web browser to perform the activation on the server, then transfer the resulting file to your PC for completion of the activation of S32 Design Studio.

Best Regards,

Mike