demo "apex_face_detection_cv" count not work

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

demo "apex_face_detection_cv" count not work

1,064 次查看
bruce_021
Contributor II

HI NXP,

I build apex_face_detection_cv and copy elf and all datas to my platform, but it could not work.

Could you help to check?

Below is the error info:

OpenCV Error: Assertion failed (u->origdata == data) in deallocate, file /home/b45336/git/vsdk/opencv_src/modules/core/src/ocl.cpp, line 4581
terminate called after throwing an instance of 'cv::Exception'
what(): /home/b45336/git/vsdk/opencv_src/modules/core/src/ocl.cpp:4581: error: (-215) u->origdata == data in function deallocate

Aborted

My platform is SBC-s32v234, sdk version is: VisionSDK_S32V2xx_RTM_1_0_0.

Thanks.

标签 (1)
标记 (3)
0 项奖励
回复
1 回复

927 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

this SDK version is old  and I don't have it. You can try the latest version VisionSDK_S32V2xx_RTM_1_1_1 

Jiri

0 项奖励
回复