debug Error in services launch sequence:gdb server unable to start

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

debug Error in services launch sequence:gdb server unable to start

4,013件の閲覧回数
qinyun_sun
Contributor I

Error in services launch sequence
There appears to be an issue with your network settings.
The gdb server was unable to start a required server component.Please contact technical support.

my pc system is windows 10  64bit 

we have the same problem, when use devkit-mpc5744p (opensda) to flash the RBF file . 

An error - while flashing the RBF file on devkit-mpc5744p  

i do not understand the feedback from this:"The issue is that the computer name was incorrect in my /etc/hosts file (linux)." my pc is windows.   

gdb server unable to start 

5744问题.JPG

debug配置.JPG

ラベル(1)
タグ(4)
0 件の賞賛
返信
1 返信

3,962件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

Can you please share debug console output

pastedImage_2.png

or try to start gdb server from command line? 

pastedImage_1.png

Jiri

0 件の賞賛
返信