com port not detecting

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

com port not detecting

3,163件の閲覧回数
Anjalipurushothaman
Contributor III

while debudding using Open sda debugger, in the drop down option com port is disbaled.

Evaluation board- s32k3x4evb-T172

Software ide - S32design studio for s32 platform (3.5 version)

 

Please find the attached .

0 件の賞賛
返信
3 返答(返信)

3,108件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

debugger integrated on S32K34x EVB is Embedded PE Micro Multilink FX: 

jiri_kral_0-1694448172621.png

 

0 件の賞賛
返信

3,103件の閲覧回数
Anjalipurushothaman
Contributor III

The board has an open sda port available, how can I use this on board debugging port instead of PE micro debugger?

This evb manual says it allows you to connect your development board to a host computer and use a compatible Integrated Development Environment (IDE)?

0 件の賞賛
返信

3,097件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

Did you tried the option shown above? There is no OpenSDA debugger as is known on S32K1xx devices. There is embedded PE Micro Multilink FX debugger integrated on the board and accessible via Micro USB. But the functionality is same - the micro USB acts as debugger and COM port. 

 

Or may be I don't get the question. 

0 件の賞賛
返信