can not open the s32ds with errors

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

can not open the s32ds with errors

1,052 次查看
nick1130
Contributor I

java.lang.IllegalArgumentException: Argument cannot be null
at org.eclipse.swt.SWT.error(SWT.java:4514)
at org.eclipse.swt.SWT.error(SWT.java:4448)
at org.eclipse.swt.SWT.error(SWT.java:4419)
at org.eclipse.swt.widgets.Widget.error(Widget.java:482)
at org.eclipse.swt.widgets.Widget.checkParent(Widget.java:291)
at org.eclipse.swt.widgets.Widget.<init>(Widget.java:158)
at org.eclipse.swt.widgets.Control.<init>(Control.java:110)
at org.eclipse.swt.widgets.Scrollable.<init>(Scrollable.java:82)
at org.eclipse.swt.widgets.Composite.<init>(Composite.java:96)
at org.eclipse.e4.ui.workbench.renderers.swt.ElementReferenceRenderer.createWidget(ElementReferenceRenderer.java:58)
at org.eclipse.e4.ui.internal.workbench.swt.PartRenderingEngine.createWidget(PartRenderingEngine.java:975)
at org.eclipse.e4.ui.internal.workbench.swt.PartRenderingEngine.safeCreateGui(PartRenderingEngine.java:651)
at org.eclipse.e4.ui.internal.workbench.swt.PartRenderingEngine.safeCreateGui(PartRenderingEngine.java:757)
at org.eclipse.e4.ui.internal.workbench.swt.PartRenderingEngine.access$0(PartRenderingEngine.java:728)
at org.eclipse.e4.ui.internal.workbench.swt.PartRenderingEngine$2.run(PartRenderingEngine.java:722)
at org.eclipse.core.runtime.SafeRunner.run(SafeRunner.java:42)
at org.eclipse.e4.ui.internal.workbench.swt.PartRenderingEngine.createGui(PartRenderingEngine.java:706)
at org.eclipse.e4.ui.internal.workbench.PartServiceImpl.createElement(PartServiceImpl.java:1257)
at org.eclipse.e4.ui.internal.workbench.PartServiceImpl.showPart(PartServiceImpl.java:1218)
at org.eclipse.ui.internal.WorkbenchPartReference.getPart(WorkbenchPartReference.java:401)
at org.eclipse.ui.internal.WorkbenchPage.busyShowView(WorkbenchPage.java:1278)
at org.eclipse.ui.internal.WorkbenchPage$12.run(WorkbenchPage.java:4316)
at org.eclipse.swt.custom.BusyIndicator.showWhile(BusyIndicator.java:70)
at org.eclipse.ui.internal.WorkbenchPage.showView(WorkbenchPage.java:4312)
at org.eclipse.ui.internal.ide.IDEWorkbenchPlugin$1.run(IDEWorkbenchPlugin.java:367)
at org.eclipse.swt.widgets.Display.runTimer(Display.java:4337)
at org.eclipse.swt.widgets.Display.messageProc(Display.java:3426)
at org.eclipse.swt.internal.win32.OS.DispatchMessageW(Native Method)
at org.eclipse.swt.internal.win32.OS.DispatchMessage(OS.java:2552)
at org.eclipse.swt.widgets.Display.readAndDispatch(Display.java:3822)
at org.eclipse.swt.widgets.Display.release(Display.java:3881)
at org.eclipse.swt.graphics.Device.dispose(Device.java:298)
at org.eclipse.ui.internal.ide.application.IDEApplication.start(IDEApplication.java:154)
at org.eclipse.equinox.internal.app.EclipseAppHandle.run(EclipseAppHandle.java:196)
at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.runApplication(EclipseAppLauncher.java:134)
at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.start(EclipseAppLauncher.java:104)
at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:388)
at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:243)
at sun.reflect.NativeMethodAccessorImpl.invoke0(Native Method)
at sun.reflect.NativeMethodAccessorImpl.invoke(NativeMethodAccessorImpl.java:62)
at sun.reflect.DelegatingMethodAccessorImpl.invoke(DelegatingMethodAccessorImpl.java:43)
at java.lang.reflect.Method.invoke(Method.java:498)
at org.eclipse.equinox.launcher.Main.invokeFramework(Main.java:673)
at org.eclipse.equinox.launcher.Main.basicRun(Main.java:610)
at org.eclipse.equinox.launcher.Main.run(Main.java:1519)

28061828-d5f4-4353-9ccd-8b09c7f1a155.jpg

 

0 项奖励
回复
1 回复

988 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

sorry for delay, if the issue remains, can you please share log file from your workspace? That one which is mentioned on your screenshot. 

0 项奖励
回复