build graph project error info, /bin/bash: line 1: 67340 Segmentation fault

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

build graph project error info, /bin/bash: line 1: 67340 Segmentation fault

1,424 次查看
caihuanming
Contributor I

When I build graph project , the problem always happens. whats wrong with it ?

the build error info :

Current SDK ROOT is /home/ds/WorkGit/nxp_moorechip/S32DS/s32v234_sdk
arm32/sa CC static_ov10640_12bcomb_surround-c.o
arm32/sa LD sequencer.elf <= static_ov10640_12bcomb_surround-c.o ../../../../../isp/firmware/build-v234ce-gnu-linux-d/libsequencer.a
------------------------------------------------------------
generating: sequencer.run
dos2unix: converting file sequencer.run to Unix format...
generating gcc: sequencer_srec.c
sequencer.run
.C0_headdep.mk: updating sequencer_srec-c.C0.d
.C0_headdep.mk: updating ov10640_12bcomb_surround-c.C0.d
.C6_headdep.mk: updating static_ov10640_12bcomb_surround-c.C6.d
Current SDK ROOT is /home/ds/WorkGit/nxp_moorechip/S32DS/s32v234_sdk
ipus/sa AS ipus.elf <= ../../../../../isp/kernels/ov10640_isp_multi/src/lut4k.ipus ../../../../../isp/kernels/ov10640_isp_multi/src/tee.ipus ../../../../../isp/kernels/ov10640_isp_multi/src/endian.ipus ../../../../../isp/kernels/ov10640_isp_multi/src/exposure.ipus ../../../../../isp/kernels/ov10640_isp_multi/src/rgb2y_lut.ipus ../../../../../isp/kernels/ov10640_isp_multi/src/debayer.ipus ../../../../../isp/kernels/ov10640_isp_multi/src/debayer_even.ipus ../../../../../isp/kernels/ov10640_isp_multi/src/debayer_odd.ipus ../../../../../isp/kernels/ov10640_isp_multi/src/copy_replicate3x.ipus ../../../../../isp/kernels/ov10640_isp_multi/src/yuv444touyvy.ipus ../../../../../isp/kernels/ov10640_isp_multi/src/probe2bgr_2x.ipus ../../../../../isp/kernels/ov10640_isp_multi/src/planar444_to_interleaved.ipus ../../../../../isp/kernels/ov10640_isp_multi/src/debayer_rgb_simple_interleaved.ipus
------------------------------------------------------------
ipuv/sa AS ipuv.elf <= ../../../../../isp/kernels/ov10640_isp_multi/src/tonemap_12b.ipuv ../../../../../isp/kernels/ov10640_isp_multi/src/rgb2y.ipuv ../../../../../isp/kernels/ov10640_isp_multi/src/rgb2uyvy.ipuv ../../../../../isp/kernels/ov10640_isp_multi/src/rgb_compress.ipuv ../../../../../isp/kernels/ov10640_isp_multi/src/rgb_compress_rgba.ipuv
------------------------------------------------------------
-------------------------------------
Creating kmem.elf
ld -T ../../../../../build/nbuild/isp_tools/M0_data.ld --accept-unknown-input-arch \
ipus.elf ipuv.elf -o kmem.elf || { exit 1; }
/bin/bash: line 1: 67596 Segmentation fault ld -T ../../../../../build/nbuild/isp_tools/M0_data.ld --accept-unknown-input-arch ipus.elf ipuv.elf -o kmem.elf
make: *** [../../../../../build/nbuild/isp_tools/isp-graphgen.mk:84: kmem.elf] Error 1

标记 (4)
0 项奖励
回复
2 回复数

1,308 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

what is your VSDK version and host OS? 

Jiri

0 项奖励
回复

1,308 次查看
caihuanming
Contributor I

VSDK 1.2  and host OS  is ubuntu18.0

0 项奖励
回复