brief Defines for user pin and port configurations

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

brief Defines for user pin and port configurations

跳至解决方案
2,876 次查看
jetty1012
Contributor II

What do I have to configure to generate the code on the left side?

The right side is mine at present. I'm using S32 DS v3.5

File: \board\Siul2_Port_Ip_Cfg.h

jetty1012_0-1683808329647.jpeg

 

Thanks,

Jetty

0 项奖励
回复
1 解答
2,869 次查看
mikedoidge
NXP Employee
NXP Employee

Hello @jetty1012,

If you use the PINs tool, you can configure each of these pins and the names that you use for the Identifier field will appear in the generated code. If you select the 'Code Preview' tab, then you can see the changes that you make appear in the code files.

mikedoidge_0-1683823058291.png

 

Best Regards,

Mike

在原帖中查看解决方案

2 回复数
2,439 次查看
RogerFranca
Contributor II

For some reason, for me, PTA HIGH generates a compilation error, the autogenerated code itself already generates the error.

I checked all the files and the error really doesn't make sense because the other ports don't present this error.

RogerFranca_0-1706807412530.png

 

0 项奖励
回复
2,870 次查看
mikedoidge
NXP Employee
NXP Employee

Hello @jetty1012,

If you use the PINs tool, you can configure each of these pins and the names that you use for the Identifier field will appear in the generated code. If you select the 'Code Preview' tab, then you can see the changes that you make appear in the code files.

mikedoidge_0-1683823058291.png

 

Best Regards,

Mike