Why can't I install FreeRTOS for S32CC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Why can't I install FreeRTOS for S32CC

ソリューションへジャンプ
9,060件の閲覧回数
cxc
Contributor I

2022-05-31 131243.png

我想知道我缺少哪些插件,RTD? 或别的什么

 

0 件の賞賛
返信
1 解決策
7,974件の閲覧回数
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @zhengeric

You need to install the SW32K3_RTD_4.4_1.0.0_DS_updatesite_D2110, as mentioned in the release notes.

As per your installation details : 

You have these RTD packages
Package: SW32K3 RTD 4.4 version 0.8.1 D2011; Version: 0.8.1; Build id: 202011302212
Package: S32K3 RTD AUTOSAR 4.4 Version 2.0.0; Version: 2.0.0; Build id: 202203311410

But, I think you are missing the required RTD package SW32K3_RTD_4.4_1.0.0_DS_updatesite_D2110.

Please can you try to install the particular RTD version and check if it works. 

Thank you. Best regards, 

- Mehul

- Mehul 

元の投稿で解決策を見る

0 件の賞賛
返信
13 返答(返信)
7,881件の閲覧回数
RachelGomez123
Contributor I

It's difficult to say without more information about the specific issues you're facing, but here are a few possible reasons why you might be having trouble installing FreeRTOS for S32CC:

Incompatible versions: Make sure you are downloading the correct version of FreeRTOS that is compatible with your version of S32CC. FreeRTOS is often distributed as a package that includes source code, header files, and libraries for different platforms and architectures, so it's important to choose the correct version for your system.

Missing dependencies: Some versions of FreeRTOS require specific dependencies, such as certain versions of compilers, libraries, or SDKs. Make sure that you have all the necessary dependencies installed on your system before attempting to install FreeRTOS.

Configuration issues: Make sure that you have configured your project correctly to use FreeRTOS. This may involve setting certain compiler options, including specific header files, or modifying linker scripts to include the FreeRTOS library.

If you are still having trouble installing FreeRTOS for S32CC, it might be helpful to consult the official documentation or forums for the software to see if there are any known issues or workarounds. Additionally, you might consider reaching out to the software vendor or a community of users for support.

 

Regards,

Rachel Gomez

0 件の賞賛
返信
8,958件の閲覧回数
chrome777
Contributor I

pls. can you tell me where you found this plugin? I also need

0 件の賞賛
返信
9,046件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

You will need to install the RTD package first. It is required by the FreeRTOS package.

0 件の賞賛
返信
7,995件の閲覧回数
zhengeric
Contributor I

Hello, Mike

  I met the same problem. I need to install FreeRTOS for S32K3 (SW32K3_freertos_10_4_5_uos_1_0_0_ds_updatesite_d2101.zip). I also installed the plug-in as described in ReleaseNote. But I still get the warning information

S32DS_FreeRTOS_Install_Issue

Here is my Installation Details:

Package: RTD S32K1 1.0.0; Version: 1.0.0; Build id: 202108251230
Package: AMMCLIB for S32S2xx devices; Version: 1.1.27; Build id: 202112140821
Package: S32K1xx development package; Version: 3.4.1; Build id: 202106101451
Package: S32SDK S32K1XX RTM 4.0.3; Version: 4.0.3; Build id: 202205261513
Package: NXP GCC for Arm Embedded Processors Build 1574; Version: 1574; Build id: 202005201521
Package: NXP GCC for Arm Embedded Processors v10.2 build 1728; Version: 1728; Build id: 202109281337
Package: GDB Client for ARM Embedded Processors 9.2 Build 1701; Version: 1701; Build id: 202012011653
Package: S32G development package; Version: 3.4.3; Build id: 202112151558
Package: S32R45 development package; Version: 3.4.1; Build id: 202104231730
Package: SW32K3 RTD 4.4 version 0.8.1 D2011; Version: 0.8.1; Build id: 202011302212
Package: S32SDK S32K1XX RTM 4.0.1; Version: 4.0.1; Build id: 202010271245
Package: S32 Design Studio Platform Tools package; Version: 3.4.3; Build id: 202112151555
Package: S32K3 RTD AUTOSAR 4.4 Version 2.0.0; Version: 2.0.0; Build id: 202203311410
Package: Radar extension package for S32R45; Version: 1.1.0; Build id: 202105111459
Package: S32 Design Studio Platform package; Version: 3.4.3; Build id: 202112151555
Package: NXP GCC for Arm Embedded Processors v6.3 build 2017 with EWL2; Version: 2017; Build id: 202005201521
Package: S32 SDK for S32V23x Version 1.0.0 RTM with Patch 1.0.1; Version: 1.0.1; Build id: 202011191547
Package: S32K3xx development package; Version: 3.4.3; Build id: 202205270927
Package: AMMCLIB for S32K14x devices; Version: 1.1.27; Build id: 202112140821
Package: AMMCLIB for S32K11x devices; Version: 1.1.27; Build id: 202112140821
Package: NXP GCC for Arm Embedded Processors Build 1620; Version: 1620; Build id: 202005201521
Package: S32 SDK for S32S247TV Version 0.8.0 EAR with Patch 0.8.1; Version: 0.8.1; Build id: 202011191547
Package: S32K1 RTD AUTOSAR 4.4 Version 1.0.1; Version: 1.0.1; Build id: 202203021500
Package: S32 RTD AUTOSAR 4.4 Version 3.0.2; Version: 3.0.2; Build id: 202204011127
Package: Vision extension package for S32V23x; Version: 1.3.0; Build id: 202102122002
Package: NXP GCC for Arm Embedded Processors v9.2 build 1649; Version: 1649; Build id: 202005201157
Package: GNU ARM PEMicro Interface Debugging Support; Version: 5.5.7; Build id: 202304031909
Package: S32S2xxTV development package; Version: 3.4.0; Build id: 202012171332
Package: AMMCLIB for S32V234 devices; Version: 1.1.27; Build id: 202112140821
Package: S32V2xx development package; Version: 3.4.0; Build id: 202012171312

Do you know what I did wrong?Looking forward to your help, thanks!

0 件の賞賛
返信
7,975件の閲覧回数
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @zhengeric

You need to install the SW32K3_RTD_4.4_1.0.0_DS_updatesite_D2110, as mentioned in the release notes.

As per your installation details : 

You have these RTD packages
Package: SW32K3 RTD 4.4 version 0.8.1 D2011; Version: 0.8.1; Build id: 202011302212
Package: S32K3 RTD AUTOSAR 4.4 Version 2.0.0; Version: 2.0.0; Build id: 202203311410

But, I think you are missing the required RTD package SW32K3_RTD_4.4_1.0.0_DS_updatesite_D2110.

Please can you try to install the particular RTD version and check if it works. 

Thank you. Best regards, 

- Mehul

- Mehul 

0 件の賞賛
返信
7,943件の閲覧回数
zhengeric
Contributor I

Hi, @Mehul_Patel_NXP 

  I installed sw32K3_rtd_4.411.0.0_ds_updatesite_d2110 as you suggested. Then FreeRTOS can be installed normally, which helps me a lot. Thank you very much!

7,975件の閲覧回数
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @zhengeric

Please can you attach the image for the warning information image again.

As doesn't show up.


Thank you. Kind regards.

- Mehul

mehul_patel_austin_1-1683316297910.png

 

 

 

0 件の賞賛
返信
8,236件の閲覧回数
Prathyusha
Contributor II

Hello, 

Even I am facing same issue. RTD package was already installed, still seeing this error.

Could you please help me to resolve this.

Thanks.

0 件の賞賛
返信
8,227件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello @Prathyusha,

What version of the RTD did you install?

If your error is matching the one already posted in this thread, then you are trying to install the FreeRTOS v2.0.0. Looking at the release notes for this version, I see the following restriction:

Known Issues, Limitations, Notes - General:
- NXP Semiconductors S32K3 FreeRTOS version 2.0.0 is only compatible with 
  SW32K3_RTD_4.4_2.0.0_DS_updatesite_D2203.zip

 Is the version of the RTD matching this? If not, I suggest you try installing this version instead. If you don't care about which version, I noticed that there is a much newer version which may match with the RTD version you already have installed.

Best Regards,

Mike

0 件の賞賛
返信
8,196件の閲覧回数
Prathyusha
Contributor II

Hi @mikedoidge ,

I am able to install once the SW32K3_RTD_4.4_R21-11_3.0.0_CD04_D2212_updatesite has installed.

Thanks for the quick response.

BR,

Prathyusha

 

0 件の賞賛
返信
8,908件の閲覧回数
cxc
Contributor I

when i use lwip example code, why i can not select freertos as the middleware?am i miss any step?tcpip.png

0 件の賞賛
返信
8,835件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

@cxc,

Please provide the NXP device and core you are using. Also, please share the 'Installation Details' screen from the S32DS Extensions and Updates menu. Look for the blue text 'Installation Details' to the lower left.

Best Regards,

Mike

0 件の賞賛
返信
9,047件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

 

What is your target MCU? Do you have installed and updated dev package for it? 

 

Jiri

0 件の賞賛
返信