Which debugging interface is better?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Which debugging interface is better?

跳至解决方案
3,293 次查看
srikarthik0601
Contributor II

I have a S32K144-Q100 evaluation board( total newbie here). Just wanted to ask which debugging interface is better ? Segger Debugging Interface or GDB PEMicro Debugging Interface 
What will be the differences if I choose one over the another?

0 项奖励
回复
1 解答
3,230 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @srikarthik0601 

This setting enables the semi-hosting support and configures input/output to print information to the console during debugging.

  • No I/O - No printing will be done.
  • Debugger Console - The output will be printed out to the console provided by the debugger specified in the Debugger setting.
  • Real-time printf with ITM - The Instrumentation Trace Macrocell (ITM) block provides a mechanism for sending data from your target to the debugger via the SWO trade stream.

在原帖中查看解决方案

0 项奖励
回复
5 回复数
3,278 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @srikarthik0601 

As you are using an EVB, is not necessary to use an external debugger to flash programming unless you want it or require it.

Our EVB comes with an onboard debugger with OpenSDA, which provides a bridge between your computer (or other USB hosts) and the embedded target processor, which can be used for debugging, flash programming, and serial communication, all over a simple USB cable.

OpenSDA is programmed with the proprietary P&E Micro-developed bootloader. P&E Micro is the default debug interface app.

 

B.R.

VaneB

0 项奖励
回复
3,243 次查看
srikarthik0601
Contributor II
Thanks for the quick reply
0 项奖励
回复
3,244 次查看
srikarthik0601
Contributor II

srikarthik0601_0-1693832633455.png

I just wanted to know what to choose over here, PEMicro or Segger
I will go with PEMicro then. 
And also can you tell me about I/O support, Debugger Console vs real time printf with ITM

0 项奖励
回复
3,231 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @srikarthik0601 

This setting enables the semi-hosting support and configures input/output to print information to the console during debugging.

  • No I/O - No printing will be done.
  • Debugger Console - The output will be printed out to the console provided by the debugger specified in the Debugger setting.
  • Real-time printf with ITM - The Instrumentation Trace Macrocell (ITM) block provides a mechanism for sending data from your target to the debugger via the SWO trade stream.
0 项奖励
回复
3,153 次查看
srikarthik0601
Contributor II
Thank you so much!