Whether the S32 Design Studio for ARM Version 2.2 with window11?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Whether the S32 Design Studio for ARM Version 2.2 with window11?

2,733 Views
jingfang
Contributor IV

The customer uses windows 11, install "S32DS_ARM_Win32_v2.2",complie ok.

File ->  NEW -> S32DS Application Project ->S32K144 ->SDK ->SDK144_SDK 3.0.0 ->Finsh

In the process of creating a project,there are many errors,as shown below:

My computer performed the same operation with windows 10 without error.

pic(4).png

0 Kudos
Reply
3 Replies

2,392 Views
rwaghode
Contributor I

Is S32 design studio support to windows 11?

0 Kudos
Reply

2,371 Views
Mehul_Patel_NXP
NXP Employee
NXP Employee


Hi, @rwaghode , 

 

NXP support the windows and Linux version of host operating systems as listed on NXP website.

 

As mentioned here: https://www.nxp.com/design/software/development-software/s32-design-studio-ide:S32-DESIGN-STUDIO-IDE

 

 

And release notes : https://www.nxp.com/docs/en/fact-sheet/S32DS-FS.pdf

 

But, "it may work on windows 11", or may have some issues while installation, as it is not tested on Windows 11.

 

The listed operating systems on the release notes are officially supported and tested.

 

Please kindly let us know if you have any further question regarding it.

 

Thank you. Kind regards. 

 

- Mehul Patel 

0 Kudos
Reply

2,659 Views
mikedoidge
NXP Employee
NXP Employee

Hello,

"S32DS_ARM_Win32_v2.2" was never tested on Windows 11. In fact, Windows 11 did not exist yet. "S32DS_ARM_Win32_v2.2" was released on Jan 29, 2020. Windows 11 was officially released on October 5, 2021.

We cannot support OS versions for which this product was not tested.

Best Regards,

Mike

0 Kudos
Reply