What's the difference between "build-v234ce-gnu-linux-d" and "build-v234ce-gnu-linux-o"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What's the difference between "build-v234ce-gnu-linux-d" and "build-v234ce-gnu-linux-o"

2,205 Views
bruce_021
Contributor II

Hello,

What's the difference between "build-v234ce-gnu-linux-d" and "build-v234ce-gnu-linux-o"?

When should I use "build-v234ce-gnu-linux-d" to build APP and when should I use "build-v234ce-gnu-linux-o"?

Thanks.

Labels (2)
2 Replies

2,014 Views
mikedoidge
NXP Employee
NXP Employee

Hello,

The -o suffix denotes a project which was built with the compiler setting for optimized build. This means there will be no debug capability enabled in this build. It also means the memory size on the target required by the application will be smaller, depending upon which optimization level was selected.

The -d suffix denotes a project which was build with the compiler setting for debug. This means this project can be used with a debugger, but will require more memory space on the target.

As it is always important to be aware of size when developing applications for embedded systems, it is possible to develop an application which would fit onto a given MCU when optimized, but could not fit when built for debug.

Hope it helps,

Mike

2,014 Views
bruce_021
Contributor II

Thanks very much.

0 Kudos
Reply