What packages needed for a T-Box generic bringup " HelloWorld" using S32 DS3.5 ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What packages needed for a T-Box generic bringup " HelloWorld" using S32 DS3.5 ?

2,719 Views
Ahmed_Saber
Contributor I

Hello,

 

I need to install the packages dedicated to the T-Box development, it is the first bring-up for the "Helloworld"
Not sure which packages I have to install and how ( I mean which SDKs, which BSPs)
Appreciate any help

 

Thanks

0 Kudos
Reply
8 Replies

2,712 Views
Ahmed_Saber
Contributor I

For example in the Getting started document for the T-Box
it refers to this package

 Ahmed_Saber_0-1692452780948.png

 

But I'm not sure where can I get this package.

 



0 Kudos
Reply

2,567 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Please follow this guide:

https://www.nxp.com/webapp/Download?colCode=TP-S32K3-T-BOX-SW-ENABLEMENT-GUIDE

There's detailed description. S32DS 3.4 and RTD 1.0.0 is needed.

“Getting Started with S32K3 using S32DS at the hello world project Training Presentation” document is general one, not directly for T-Box.

Regards,

Lukas

0 Kudos
Reply

2,524 Views
Ahmed_Saber
Contributor I

Hello Lukas,

 

Thanks for the response.
but I would like to download the BSP, as I'm targetting to bring up the T box for CAN communication
Which one shall I use

0 Kudos
Reply

2,455 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @Ahmed_Saber 

just follow the document step by step. It shows which packages are needed exactly:

lukaszadrapa_0-1693196817138.png

 By the way, it's not called BSP here but rather RTD (Read Time Drivers).

Regards,

Lukas

0 Kudos
Reply

2,429 Views
Ahmed_Saber
Contributor I

Hi Lukas,

 

Again, I don't mind the instructions mentioned in the enablement guide, but as you said earlier it is something common for the S32K3, but what I'm seeking is something for the T box board
I have installed the DS3.4 with the mentioned packages
Now I need to proceed with a prepared package for the T box to not invent the wheel
As I can see here: https://www.nxp.com/design/designs/s32k3-automotive-telematics-box-t-box-reference-design-board:S32K...
There a BSP package, in my opinion, this is can be used as a base for SW building for the T box ready for the components on the board ( Trcvs...etc)

But the problem is, once I import this BSP as a project, I got this error message

2023-08-29 10_43_56-Snipping Tool.png

 Hope you get my point.

 

Regards Ahmed

0 Kudos
Reply

2,426 Views
Ahmed_Saber
Contributor I

Also,
this is the installed packages

Ahmed_Saber_0-1693298946029.png


And this the DS32 tool version I have installed

Ahmed_Saber_1-1693298993443.png

 

 

0 Kudos
Reply

2,398 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

I tested it on my side. I have almost the same SW configuration here (only a few more packages which should not be important here), I downloaded and imported S32K3_T_BOX_BSP.zip and I can open the configuration tool and I can compile the project.

Is that really original project from S32K3_T_BOX_BSP.zip? Have you made any changes there?

https://www.nxp.com/webapp/Download?colCode=S32K3-T-BOX-BSP

My SW:

lukaszadrapa_0-1693379242351.png

Regards,

Lukas

0 Kudos
Reply

2,577 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @Ahmed_Saber 

let me check this with owners of the T-Box. I can see two getting started documents and SW enablement guide and all of them says something different. I'm sure that specific RTD version needs to be used.

Generally, the RTD can be downloaded from S32K3 Standard Software Package. The link can be found here in the mentioned document:

lukaszadrapa_2-1692684974517.png

this will redirect you here (RTD link highlighted)

lukaszadrapa_3-1692685019705.png

I will let you know later which version should be used exactly.

And notice that this document provides more details about the installation:

https://www.nxp.com/webapp/Download?colCode=TP-S32K3-T-BOX-SW-ENABLEMENT-GUIDE

Regards,

Lukas

 

 

 

0 Kudos
Reply