Using malloc on a S32R274 with S32 Studio

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using malloc on a S32R274 with S32 Studio

1,664件の閲覧回数
simonschoenenbe
Contributor I

I have problems to use the functions "malloc" and "calloc" on a S32R274 core0. When I use one of these functions it always ends up in the IVOR1 exception. I'm using the "ewl_c Debugger Console" library. The heap is defined as in the two linker script files attached. Do you know what I'm doing wrong? Can anybody help me?

ラベル(2)
0 件の賞賛
返信
0 返答(返信)