Hi
I am using the S32K144 EVB and I am facing an issue while debugging the code
Currently while starting a debug session the progress bar stops at 98% and nothing happens further.
I have monitored the reset line on the board , Reset LED is not high always ( Working As usual as earlier)
I tried with USB as well as 12V external supple , Same Issue
The log while downloading the elf file is as below.
Connection from "127.0.0.1" via 127.0.0.1. Connection from port "53843" to 6224
Connection from "127.0.0.1" via 127.0.0.1. Connection from port "53845" to 7224
Telnet server running on 127.0.0.1:51794
Searching for Kernel Symbols...
rsp_qC - qSymbol: 5F74785F7468726561645F63757272656E745F707472
_tx_thread_current_ptr not found. ThreadX analysis not enabled.
rsp_qC - qSymbol: 707843757272656E74544342
pxCurrentTCB not found. FreeRTOS analysis not enabled.
Unable to load libusb0.dll
Copyright 2021 P&E Microcomputer Systems,Inc.
Command Line :C:\NXP\S32DS_ARM_v2.2\eclipse\plugins\com.pemicro.debug.gdbjtag.pne_5.1.7.202112141853\win32\pegdbserver_console -device=NXP_S32K1xx_S32K144F512M15 -startserver -singlesession -serverport=7224 -gdbmiport=6224 -interface=USBMULTILINK -speed=¨
OpenSDA detected - Flash Version 1.19
CMD>RE
Initializing.
Target has been RESET and is active.
CMD>CM C:\NXP\S32DS_ARM_v2.2\eclipse\plugins\com.pemicro.debug.gdbjtag.pne_5.1.7.202112141853\win32\gdi\P&E\supportFiles_ARM\NXP\S32K1xx\freescale_s32k144f512m15_pflash_dflash_eeprom.arp
Initializing.
After this , It will hang there forever
I even tried checking the Emergency Kinetics Device Recovery by Full Chip Erase , still getting struct at 99%
Please help. Any guidance would be really helpful
已解决! 转到解答。
Hi @jiri_kral
The problem was with particular EVB , with other EVBs , I can debug without any problem
But ultimately I found the solution , I followed this thread (https://community.nxp.com/t5/S32K-Knowledge-Base/Solution-for-S32K14x-which-could-be-attached-while-...)
Thanks for support
Hi,
please try to re-install PE Micro drivers - it is part of S3DS installation with default install path located in
c:\NXP\S32DS_ARM_v2.2\Drivers\
folder. Also updating PE Micro plugin after reinstall may help:
https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Install-update-from-3rd-party-ve...
Jiri
Hi @jiri_kral
The problem was with particular EVB , with other EVBs , I can debug without any problem
But ultimately I found the solution , I followed this thread (https://community.nxp.com/t5/S32K-Knowledge-Base/Solution-for-S32K14x-which-could-be-attached-while-...)
Thanks for support