Unable to resolve Semantic errors in S32 design studio

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to resolve Semantic errors in S32 design studio

ソリューションへジャンプ
3,296件の閲覧回数
Anilpatil_SasvaAuto
Contributor III

Hello Team,

I am trying to compile the NFC reader library project. After a successful build, I did not encounter any compilation errors or warnings; however, I found two semantic errors in the Problems window.

These errors appear even after I have provided the path to include in the IDE settings. Please note that these errors will not be displayed in the Problems window unless you open the "phbalReg_S32kSpi.c" file from the DAL folder.

Please refer to the attached files for your reference

I would appreciate any solutions to resolve the symbols or errors. Thank you!

0 件の賞賛
返信
1 解決策
3,029件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

I'm not able reproduce the issue. Can you please share the screenshot with the errors and ideally with error details if there are some? 

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
2,561件の閲覧回数
Anilpatil_SasvaAuto
Contributor III

Issue resolved from my side

 

0 件の賞賛
返信
3,281件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

what's your S32DS version and target MCU? 

0 件の賞賛
返信
3,258件の閲覧回数
Anilpatil_SasvaAuto
Contributor III
S32DS version: 3.4
Target MCU:S32K144EVB
0 件の賞賛
返信
3,243件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

And which particular version of NFC Reader library are you using? 

0 件の賞賛
返信
3,211件の閲覧回数
Anilpatil_SasvaAuto
Contributor III

NFC reader library version number: aNfcRdLib_SDK_Evaluation_v2.28

0 件の賞賛
返信
3,030件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

I'm not able reproduce the issue. Can you please share the screenshot with the errors and ideally with error details if there are some? 

0 件の賞賛
返信