Unable to resolve Semantic errors in S32 design studio

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Unable to resolve Semantic errors in S32 design studio

跳至解决方案
1,479 次查看
Anilpatil_SasvaAuto
Contributor III

Hello Team,

I am trying to compile the NFC reader library project. After a successful build, I did not encounter any compilation errors or warnings; however, I found two semantic errors in the Problems window.

These errors appear even after I have provided the path to include in the IDE settings. Please note that these errors will not be displayed in the Problems window unless you open the "phbalReg_S32kSpi.c" file from the DAL folder.

Please refer to the attached files for your reference

I would appreciate any solutions to resolve the symbols or errors. Thank you!

0 项奖励
回复
1 解答
1,212 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

I'm not able reproduce the issue. Can you please share the screenshot with the errors and ideally with error details if there are some? 

在原帖中查看解决方案

0 项奖励
回复
6 回复数
744 次查看
Anilpatil_SasvaAuto
Contributor III

Issue resolved from my side

 

0 项奖励
回复
1,464 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

what's your S32DS version and target MCU? 

0 项奖励
回复
1,441 次查看
Anilpatil_SasvaAuto
Contributor III
S32DS version: 3.4
Target MCU:S32K144EVB
0 项奖励
回复
1,426 次查看
jiri_kral
NXP Employee
NXP Employee

And which particular version of NFC Reader library are you using? 

0 项奖励
回复
1,394 次查看
Anilpatil_SasvaAuto
Contributor III

NFC reader library version number: aNfcRdLib_SDK_Evaluation_v2.28

0 项奖励
回复
1,213 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

I'm not able reproduce the issue. Can you please share the screenshot with the errors and ideally with error details if there are some? 

0 项奖励
回复