UART Buffer Merge Issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

UART Buffer Merge Issue

870件の閲覧回数
Bhuvaneshwaran_K
Contributor II

We have two separate message buffers which are transmitted in a periodic manner. The two data buffers are getting merged after a period of time, say 10 mins. Would like to understand the resolution in this regard.

Buffer 1 : aa 03 00 21 00 64 00 00 00 00 42 63 29 16 42 65 a1 30 42 38 d7 94 42 63 29 16 00 00 00 00 00 00 00 00 01 00 01

Buffer 2 : aa 01 00 03 f1 95 22 54

Merged data buffer(Issue) : aa 03 00 21 00 64 00 00 00 00 42 62 aa aa 42 65 a1 30 42 38 d7 94 42 63 a7 82 00 00 00 00 00 00 00 00 01 00 01 aa 01 00 03 f1 95 22 54 

Need your assistance at the earliest as possible.

0 件の賞賛
返信
0 返答(返信)