The Problems of PA_RSDK_RTM_1_1_1 after Compiled

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The Problems of PA_RSDK_RTM_1_1_1 after Compiled

949 Views
wanglongfeilf
Contributor I

Compile and write flash under the default parameters are without any problems.but When I modify some of the macro definition about the compiler,It appeared some problems that Progress of Flash write Keeps in 99% of the state.I don't know what is the problem.

The modified macro definition:

pastedImage_1.png

Console information:

Connection from "127.0.0.1" via 127.0.0.1
Telnet server running on 127.0.0.1:51794
Copyright 2017 P&E Microcomputer Systems,Inc.
Command Line :D:\NXP\S32DS_Power_v2017.R1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_1.7.5.201807182113\win32\pegdbserver_power_console -device=S32R274 -startserver -singlesession -serverport=7224 -gdbmiport=6224 -interface=USBMULTILINK -speed=4100 -p

CMD>RE

Initializing.
S32R274 Device detected.
Target has been RESET and is active.
CMD>CM D:\NXP\S32DS_Power_v2017.R1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_1.7.5.201807182113\win32\gdi\P&E\nxp_s32r274_1x32x488k_cflash.pcp

Initializing.
S32R274 Device detected.
Initialized.

;version 1.03, 12/13/2016, Copyright P&E Microcomputer Systems, www.pemicro.com [S32R274_1.9meg]

;device NXP, S32R274, 1x32x488k, desc=CFlash

;begin_cs device=$00F98000, length=$001E8000, ram=$40000000

Loading programming algorithm ...

WARNING - Selected .PCP file has been modified. CRC16 = $50FE
Done.
Programming sequency is : erase, blank check, program, and verify {default}
CMD>VC
Verifying object file CRC-16 to device ranges ...
block 01000000-0100032D ...
Ok.
block 01000330-0100034F ...
Ok.
block 0103D800-0103DA85 ...
Ok.
block 0103DA90-01041FAF ...
Ok.
block 01042000-010420F3 ...
Ok.
block 01042100-0105F057 ...
Ok.
block 0107DC00-0107DCFF ...

note:it has no problem during The building process   Console information Indicators that it stays in the final process of flash piece of writing

Labels (2)
0 Kudos
Reply
0 Replies