The GDB Server was not able to establish a connection to the target processor.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

The GDB Server was not able to establish a connection to the target processor.

2,791 次查看
feng_ang
Contributor II

Error in services launch sequence The GDB Server was not able to establish a connection to the target processor. Please check your connections and power. Verify that the launch settings in the Debug Configuration are accurate. To run simultaneous debug sessions, please specify a unique Server Port and GDBMI Port.

 

标记 (2)
2 回复数

2,778 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

power supply and probe connection is okay (there are two micro USB connectors)? Do you have chance test it with different board? 

2,774 次查看
feng_ang
Contributor II

屏幕截图 2023-02-20 232713.png

Hi

Thank you for your reply.

There is only one micro USB connector for each board. I don't know if this is normal for power supply and probe. And I have two MPC5748 boards. I have tested them, and the results will show that error. Is it the problem of GBD setting?