Slow build time with S32DS for ARM V2.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Slow build time with S32DS for ARM V2.0

3,620 Views
riccardolalli
Contributor I

Hello,
I just installed the new S32DS for ARM 2.0 and updated to 2.1, but I horribly noticed that building a project became really slow when compared to 1.3 version.
New version is about 10 times slower than the previous one.
I verified this by compiling the same example hello project in both environments (the project was created in 1.3 version and then copied in the 2.0 workspace folder).
I currently have both installed in my pc, and the only addition I made to the clean install was the subversive SVN plugin.
Has anyone experienced the same issue?

0 Kudos
Reply
4 Replies

3,127 Views
stanish
NXP Employee
NXP Employee

Hello Kate,

S32DS build time has no dependency on network. Perhaps the customer has some network services running which causes an additional build time delays.

What is the time difference between S32DS ARM v2.0 vs.1.3 they observe on their machine?

Regarding SVN plugin: it's not part of the default installation and needs to be added via  "Install New Software" Eclipse Updater:

 pastedImage_1.png

Hope it helps.

Stan

0 Kudos
Reply

3,126 Views
stanish
NXP Employee
NXP Employee

Hi Riccardo,

Thanks for the feedback.

I've just made a quick comparison  v1.3 vs. v2.0 + Update 1 and S32DS ARM v2.0 build time is faster so I see completely opposite results:

Hello Example:

pastedImage_3.png

FlexCAN encrypted SDK example:

pastedImage_2.png

Actually the build speed comparison is part of our test suite before release. 

I'll check with SVN plugin - is it installed on both versions?

Regards,

Stan

0 Kudos
Reply

3,126 Views
leekate-b45752
NXP Employee
NXP Employee

Hello Stanislav, 

Customer reported same as the above question, slow building time of S32 DS v2.0 comparing to v1.3. 

When they tried to build with network connection, it was too slow, but it gets faster without network connection. Is there any relation to building? Also could you guide about how to check the SVN plugin?

Best regards,

Kate Lee

0 Kudos
Reply

3,126 Views
riccardolalli
Contributor I

Hello Stan,

Yes, I installed it on both versions.

Good news however, I don't know what happened from last time (except for a weekend :smileyhappy:), but today the issue has disappeared. Now I too get slightly faster compilation times than the older version.

Thank you,

Riccardo

0 Kudos
Reply