SDK cannot be found when creating a new Application project on S32DS3.5

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SDK cannot be found when creating a new Application project on S32DS3.5

ソリューションへジャンプ
2,703件の閲覧回数
ukn
Contributor I

I recently installed S32DS3.5 and the attached image contains the  all the packages I installed along with S32DS. When I try to create an application project, I cannot see any SDK in it. Also, when I try to create a new project from example, I cannot see any examples. How do I get the SDK? should I install anything else?

 

ukn_0-1695309485219.png

 

0 件の賞賛
返信
1 解決策
2,629件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @ukn 

I ask you to please provide an image of the information provided in the installation details. This situation usually happens when it is not installed all the necessary packages or if you do not have the right version of these. 

 

B.R.

VaneB

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,209件の閲覧回数
terry-1987
Contributor I

how you fix the issue?

0 件の賞賛
返信
2,630件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @ukn 

I ask you to please provide an image of the information provided in the installation details. This situation usually happens when it is not installed all the necessary packages or if you do not have the right version of these. 

 

B.R.

VaneB

0 件の賞賛
返信
2,624件の閲覧回数
ukn
Contributor I

Hi @VaneB ,

 

I reinstalled the S32DS3.5 and the related packages and it fixed the issue. 

Thanks

0 件の賞賛
返信