S32k144 LPSPI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32k144 LPSPI

2,845 Views
wanglijun
Contributor II

Hello,

I have a question about LPSPI module in S32DS.

In S32DS code, there is a function: LPSPI_DRV_MasterTransferBlocking, it includes both transmission and reception.

But I just only need transmission or reception.

How to use the function?

@

Tags (3)
0 Kudos
Reply
3 Replies

2,720 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

when SPI master transmits a data, SPI slave sends a data back to master at the same time. This is a nature of the SPI interface. So, when you want to only transmit a data by master, you will always receive data from slave. You can just disregard such data. When you want to receive a data from slave, master must send some data to slave, so the slave can send the data back. Solution for this is to send a dummy data to slave.

Regards,

Lukas

0 Kudos
Reply

2,720 Views
wanglijun
Contributor II

Hello Lukas,

Thank you for the replying!

If I only want to receive the data, how the function should be called?

Additionally, If I want to receive by DMA, which function should be called?

0 Kudos
Reply

2,720 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

If you want to receive a data from slave, you need to transmit dummy data (like 0xFF), so the slave can clock out the data.

There's an example lpspi_dma:

c:\NXP\S32DS_ARM_v2.2\S32DS\software\S32SDK_S32K1xx_RTM_3.0.0\examples\S32K144\driver_examples\communication\lpspi_dma\

Regards,

Lukas

0 Kudos
Reply