S32k144 - DMA Interrupt

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32k144 - DMA Interrupt

2,695件の閲覧回数
Raphael2
Contributor III

Hello,

I tried to change the processor in an existing project with this guide:

https://community.nxp.com/t5/S32K-Knowledge-Base/SENT-receiver-for-S32K118-Design-Studio/ta-p/112735...

 

The "old" controller was the S32k118 and the "new" the S32k144.

 

But when I build it I get the following Errors because of the DMA interrupt.

Raphael2_1-1626445166751.png

Does the suggested ISPR the same as IPR, or with what should I replace it?

 

Best regards

Raphael

 

 

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,669件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Could you specify, which example code you have used as a template for porting of mentioned example code? Thanks

0 件の賞賛
返信

2,664件の閲覧回数
Raphael2
Contributor III

Hi,

I wanted to delete my question, but I didn't find an option to do so.

Best regards

0 件の賞賛
返信