S32ds 3.4 Linux debug problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32ds 3.4 Linux debug problem

2,723 次查看
FaustoPignatta
Contributor I
Hi,
I debug my s32k148 application with USB-Multilink in windows without problem.
But if I try it in Linux (Ubuntu) S32DS doesn't see any debugger connected.
I've downloaded and installed Linux drivers provided by pemicro.
Some ideas to resolve this issue?
Thanks

Fausto
0 项奖励
回复
3 回复数

2,694 次查看
jiri_kral
NXP Employee
NXP Employee

Hi Fausto, 

are you using virtual machine or real one? Is the PE Micro listed if you run lsusb command? 

 

Jiri

0 项奖励
回复

2,550 次查看
FaustoPignatta
Contributor I

I'm using virtual machine. Yes Pe mricro is listed when I try lsusb command.

Thanks

0 项奖励
回复

2,642 次查看
MateoSegura413
Contributor III

@jiri_kral I am having the same issue. Yes the device shows up under lsusb. Could you give me some guidance as to how I can use the PE micro debugger under linux?

Thanks in advance!

 

0 项奖励
回复