S32V234 VSDK isp_ov10640_quad work with max96705

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32V234 VSDK isp_ov10640_quad work with max96705

2,257件の閲覧回数
liujialu_2024
Contributor III

S32V234 VSDK demo 'isp_ov10640_quad' work with "max9286+max9271*4", but my camera's serializer is "max96705", ii2c read serializer and OV16040 CHIP_ID failed, detail information in attached file.

debug environment:

          hardware: S32V234EVB + MAX9286S32V234DB + LI-OV10640-490-GMSL-055H

          software: S32V234 VSDK  isp_ov10640_quad demo。

Any clear difference with max9271 & max96705? datasheet said they arm compatible.

ラベル(3)
0 件の賞賛
返信
2 返答(返信)

1,597件の閲覧回数
xiafeng_luo
Contributor I

hi,i met the same questions. After one year later ,NXP still not solve this problem...i am so surprised.  

0 件の賞賛
返信

1,597件の閲覧回数
KushalShahNXP
NXP Employee
NXP Employee

Hi,

This is not the correct community to post S32V2 questions. 

Moreover, we have stopped supporting S32V2 community group. But we still support S32V2 question using our ticketing system.

For future questions, please create the request at www.nxp.com/support using Support Requests option. Our experts will help you.

 

Thank you for understanding.

 

Regards,

Kushal

0 件の賞賛
返信