S32R45 Evaluation Board External DRAM Initialization

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32R45 Evaluation Board External DRAM Initialization

2,144 Views
ssong
Contributor II

S32R45 Evaluation Board has an external DRAM and it should be initialized in M7 bootloader

DDR tool in S32DS has been used to generate ddr-related code and kept the default configuration.

ssong_0-1654229069513.png

ddr_init() function was located in SysDal_InitBlockOne. There is a struct which is accessed by ddr_init's subfunction. but 0x4007C604, 0x4007C608 doesn't seem to be right position in S32R45 so that we can't access the below registers which starts from 0x403C0000(UMCTL2_REGS BASE_ADDRESS)

ssong_1-1654229326976.png

Could you guide us to resolve this?

 

0 Kudos
Reply
2 Replies

2,075 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

This looks like a platform setup issue.

I will check who can handle this query.

Best regards,

Peter

0 Kudos
Reply

2,140 Views
ssong
Contributor II

If you have an example project for external dram initialization, It could be the best.

0 Kudos
Reply