S32R45 Evaluation Board External DRAM Initialization

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32R45 Evaluation Board External DRAM Initialization

2,135件の閲覧回数
ssong
Contributor II

S32R45 Evaluation Board has an external DRAM and it should be initialized in M7 bootloader

DDR tool in S32DS has been used to generate ddr-related code and kept the default configuration.

ssong_0-1654229069513.png

ddr_init() function was located in SysDal_InitBlockOne. There is a struct which is accessed by ddr_init's subfunction. but 0x4007C604, 0x4007C608 doesn't seem to be right position in S32R45 so that we can't access the below registers which starts from 0x403C0000(UMCTL2_REGS BASE_ADDRESS)

ssong_1-1654229326976.png

Could you guide us to resolve this?

 

0 件の賞賛
返信
2 返答(返信)

2,066件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

This looks like a platform setup issue.

I will check who can handle this query.

Best regards,

Peter

0 件の賞賛
返信

2,131件の閲覧回数
ssong
Contributor II

If you have an example project for external dram initialization, It could be the best.

0 件の賞賛
返信