S32M RTD support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32M RTD support

7,000件の閲覧回数
hns80
Senior Contributor I

Version 3.0.0 P07 claims to support S32M. I installed it, but cannot select anything other than S32K when I create a new project. There isn't any example code available, either. 

How can I get a version of the RTDs that supports the S32M?

 

0 件の賞賛
返信
3 返答(返信)

6,937件の閲覧回数
hns80
Senior Contributor I

When I try to install these, I receive an error:

Operation details Software being installed: com.nxp.RTD.S32M276.root.feature.feature.group 3.0.0.202303311831 Missing requirement: com.nxp.RTD.S32M276.root.feature.feature.group 3.0.0.202303311831 requires 'org.eclipse.equinox.p2.iu; com.nxp.s32ds.s32m2.dev.feature.feature.group 1.0.0' but it could not be found

 

I have the following installed:

RTD S32M276 3.0.0.202306300010 com.nxp.RTD.S32M276.feature.feature.group NXP Semiconductors, Inc.
S32 Design Studio 3.5.3.202306291736 com.nxp.s32ds.platform.ide.feature.feature.group NXP
S32 Design Studio Tools 3.5.3.202306291736 com.nxp.s32ds.platform.ide.tools.feature.feature.group NXP
S32DS Product 3.5.0.202207261815 com.nxp.s32ds.platform.ide.product NXP

What am I missing?

 

0 件の賞賛
返信

6,921件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Thanks for the information.

The missing package "com.nxp.s32ds.s32m2.dev.feature.feature.group 1.0.0" is the development package for S32M platforms. It seems that it is not installed on your setup.

If you cannot find it on your available SW, then help us contacting your local NXP FAE/DBM, for them to verify if your account has the available information.

Please, let us know.

0 件の賞賛
返信

6,958件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Once you add the "SW32K3_RTD_R21-11_3.0.0_P07_D2306_DS_updatesite.zip" to S32DS v3.5 you should see both S32K3 and S32M2 RTD's. You should install the S32M RTD itself. The RTD version supports the platform, but it is through a different package, as seen below:

DanielAguirre_0-1689272633402.pngDanielAguirre_0-1689272633402.png

Have you installed these S32M specific packages?

Please, let us know.

0 件の賞賛
返信