S32KXX Development Package Could Not Be Installed for S32DS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32KXX Development Package Could Not Be Installed for S32DS

2,482件の閲覧回数
utkuf
Contributor I

When I try to install S32K3XX Development Package from S32DS Extensions and Updates window in S32DS.3.5, unfortunately it could not be installed, there is an error. How could I solve this issue?

0 件の賞賛
返信
3 返答(返信)

2,374件の閲覧回数
utkuf
Contributor I

I have installed successfully, however right now, I got an error like "Description Resource Path Location Type
fatal error: OsIf_Cfg.h: No such file or directory Can_Example_S32K344 line 45, external location: C:\NXP\S32DS.3.5\S32DS\software\PlatformSDK_S32K3\RTD\BaseNXP_TS_T40D34M30I0R0\include\OsIf_Internal.h C/C++ Problem"

0 件の賞賛
返信

2,354件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @utkuf 

Before running the example, a configuration needs to be generated. First, go to Project Explorer View in S32 DS and select the current project. Select the "S32 Configuration Tool" menu, then click on the desired configuration tool (Pins, Cocks, Peripherals etc...). Clicking on any one of those will generate all the components. Make the desired changes (if any), then click on the "S32 Configuration Tool->Update Code" button.

0 件の賞賛
返信

2,461件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @utkuf 

There is an S32 Design Studio 3.5.0 Development Package with support for S32K3xx devices. Did you already have it?

Take a look at this community post. Here is mentioned information about it.

Please let me know if you still have problems.

 

B.R.

VaneB

0 件の賞賛
返信